EnabledState

Description
Indicates whether the condition is enabled.
  • 0: The alarm is in the disabled state.
  • 1: The alarm is in the enabled state.
For more information, refer to TwoStateVariableType.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal