Port Configuration view
How do I open Port Configuration view?
- On the explorer bar, select
Devices. - InDevices, double-click the controller to open the device profile.
- In the device profile, selectPort Configuration.
Use the
Port Configuration
view to configure a port or ports for a controller.
Configuration options include enabling the port, viewing the status of another device linked
to and communicating with the controller, setting the speed and duplex of the port, and
viewing diagnostics for the port.Provide Feedback