Device definition dialog box
How do I
open the Device definition dialog box?
- On the explorer bar, select
Devices. - InDevices, double-click the controller to open the device profile.
- In the device profile, selectDevice definition.
Use the
Device definition
dialog box to:- View the device type.
- Configure device-specific settings.
TIP:
The available parameters are based on the device being configured. Parameters that do not
apply to the device are hidden.
Provide Feedback