Configure limit properties
Configure limit properties to manage the amount of data coming from an output.
To configure limit properties
- In theController Organizer, expand theI/O Configurationfolder, and double-click the module.
- In theModule Propertiesdialog box, expandChannels.
- Expand aCh0x, and then selectLimits.
- InLimits, fill in the parameters and selectOK.
Provide Feedback