Configure individual input channel properties
Configure the properties of the individual input channel to define the scaling and filtering for that channel.
To configure individual input channel properties:
- In theController Organizer, expand theI/O Configurationfolder, and double-click the module.
- In theModule Propertiesdialog box, expandChannels.
- Select the individual input channel.
- In theCh0xpage, fill in the parameters and selectOK.
Provide Feedback