Configure individual output channel properties
Configure the individual output channel so that it can properly connect to Current or Voltage output types and to multiple output signal ranges.
To configure individual output channel properties
- In theController Organizer, expand theI/O Configurationfolder, and double-click the module.
- In theModule Propertiesdialog box, expandChannels.
- Select the individual output channel.
- InCh0x, fill in the parameters and selectOK.
Provide Feedback