Revert to Factory Calibration Wizard

The Revert to Factory Calibration process reverts calibration gains and offsets of selected channels to factory values.
The Revert to Factory Calibration Wizard includes these parameters:
Parameter
Description
Channel
Shows the channel number.
Revert to Factory Calibration?
Select the channels to revert to factory calibration.
Calibration Range
Shows the range currently configured for the channel. Ranges display according to the
Input Range
or
Output Range
selected.
Current Calibration Gain
Shows the calibration gain value as reported by the module.
Current Calibration Offset
Shows the offset in units (ohm, mV, V, or mA) as reported by the module.
Last Calibration Date
Shows the last calibration date for the channel. The time and date listed here is based on the time on the computer running the
Logix Designer
application.
Calibration Status
Shows the status of the calibration per input range or output range and channel as the calibration occurs. Valid values include:
  • OK
  • Error
Back
Returns to the previous wizard window.
Next
Continues the process.
Stop
Stops the process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal