Configure alarm properties

Configure alarm properties to alert you when the module exceeds configured high or low limits.
To configure alarm properties:
  1. In the
    Controller Organizer
    , expand the
    I/O Configuration
    folder, and double-click the module.
  2. In the
    Module Properties
    dialog box, expand
    Channels
    .
  3. Expand the channel and select
    Alarms
    .
  4. In the
    Alarms
    page, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal