Configure the Cold Junction Compensation for thermocouples

Configure the cold junction compensation when a channel is configured for thermocouple operation.
The channel must account for the thermoelectric effect of a junction of the thermocouple field wires and the RTB terminals.
To configure the cold junction compensation for thermocouples
  1. On the tab for the device, select
    CJ Channels
    .
  2. In the
    CJ Channels
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal