View current channel calibration

Use
Calibration
to view current channel calibration. The calibration information includes:
  • Channel number of the devices.
  • Calibration range value that is currently configured for the channel.
  • Calibration gain values as reported by the device.
  • Calibration offset signed values as reported by the device.
  • Last successful calibration date.
  • Calibration status per channel.
To view current channel calibration
  1. On the tab for the device, select
    Calibration
    .
  2. In the
    Calibration
    view, view the current channel calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal