Calibration mismatch

Performing calibration can cause unexpected results if:
  • At least one channel is selected, and
  • There is a mismatch between the device listed in the application and the actual physical device, and
  • The system is active.
It is strongly recommended that you select No, check the configuration, and shut down the system before performing calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal