Alarms view parameters

The
Alarms
view (5094-IF8/IY8) includes these parameters:
Parameter
Description
Disable All Alarms
Prevents the device from generating any of the four process alarms (LL, L, H, and HH) or the rate alarm and does not allow access to any of the alarm configuration properties.
Latch Process Alarms
Instructs the device to latch any or all of the four process alarms (LL, L, H, and HH) once the alarm is triggered, even if the condition causing the alarm to occur disappears.
High High Limit
Sets the trigger point in Engineering Units. HHAlarm is set to 1 when the input signal moves above this limit.
High Limit
Sets the trigger point in Engineering Units. HAlarm is set to 1 when the input signal moves above this limit.
Low Limit
Sets the trigger point In Engineering Units. LAlarm is set to 1 when the input signal moves below this limit. The Low Alarm Limit must be >/= the Low Low Limit and < the High Limit.
Low Low Limit
Sets the trigger point in Engineering Units. LLAlarm is set to 1 when the input signal moves below this limit. The Low Alarm Limit must be greater than or equal to the Low Low Limit and less than the High Limit.
Deadband
Allows the process alarm status bits to remain set, even if the alarm condition disappears, as long as the channel data remains within plus or minus the deadband value of the process alarm. This
Deadband
value is entered in engineering units.
Enable Rate Alarm Latching
Latches the rate alarm so that it does not clear until explicitly unlatched.
Rate Alarm Limit
Sets if the rate of change between input samples on this channel exceeds the rate specified in this field in Engineering Units.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal