Points view parameters
The
Points
view includes these parameters:Parameter | Description |
|---|---|
Input Filters Off -> On/ On -> Off Filter Time | Specifies the value (in milliseconds) by which to delay the transition from off to on ( Off -> On ) and from on to off (On -> Off ). This delay is useful for filtering out transients in noisy environments. |
Latch Timestamp | Select to latch timestamp in CST or CIP Sync.
|
Enable Timestamp Capture | Selects each input point for which you want to capture Off -> On and On -> Off events. Selecting a checkbox captures the specified event for the corresponding input point. |
Chatter Detection | Detects a chattering signal from a device connected to an input point and ignores the data. Specify the acceptable number of input transitions within a specified time period before the signal is considered to be chatter:
|
Provide Feedback