Enable timestamp in CIP Sync

Enable the device to timestamp using CIP Sync when it is available. Disabling the feature timestamps using Coordinated System Timer (CST) or Coordinated Universal Time (UCT) if receiving pairs.
This parameter is available only for a 1756-IB16ISOE Revision 2 device configured for a
CIP Sync 10X FIFO Mode
or
CIP Sync Per Point
connection. The parameter is not available for Revision 1.
To enable timestamp in CIP Sync
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, select
    Latch Timestamp
    , and then select
    CIP Sync
    .
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal