Enable CST latching

Latch all Coordinated System Timer (CST) transitions so that an event is not overwritten without being acknowledged. For example, in 16-channel mode, in a sequence of events from OFF to ON to OFF, the first OFF and ON transitions are recorded while the final OFF transition is ignored. All subsequent transitions on that point are ignored until acknowledged or reset.
If this checkbox is cleared, then the second OFF transition in the example above overwrites the first OFF transition immediately, even if the controller has not yet extracted the data.
To enable CST latching
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, select
    Latch Timestamp
    , and then select
    CST
    .
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal