Enable a timestamp capture
Enable a timestampt capture to instruct the Sequence of Events device to timestamp the transitions of specific input points.
To enable a timestamp capture
- On the tab for the device, selectPoints.
- In thePointsview, in theEnable Timestamp Capturecolumn, select when to capture the timestamp for each input point:
- OFF to ON transition
- ON to OFF transition
- OFF to ON and ON to OFF transitionsTIP:Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
- SelectOKto save the changes.
Provide Feedback