Specify the output state when the controller is in Program mode
Specify the behavior of each output point when the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored, and the output behaves according to the behavior selected.
To specify the output state when the controller is in Program mode
- On the tab for the device, selectConfiguration.
- In theConfigurationview, in theOutput State During > Program Modecolumn, for each output point, select one of these options:
- Off.Output becomes 0 or OFF in Program mode.
- On.Output becomes 1 or ON in Program mode.
- Hold.Output maintains last state in Program mode.
- SelectOKto save the changes.
Provide Feedback