Specify the output state when the device is in Fault mode
Specify the behavior of each output point when a communication fault occurs and the device enters Communications Fault mode.
To specify the output state when the device is in Fault mode
- On the tab for the device, selectConfiguration.
- In theConfigurationview, in theOutput State During > Fault Modecolumn, for each output point, select one of these options:
- Off.Output becomes 0 or OFF in Communications Fault mode.
- On.Output becomes 1 or ON in Communications Fault mode.
- Hold.Output maintains current level in Communications Fault mode.
- SelectOKto save the changes.
Provide Feedback