Configuration view parameters
The
Configuration
view includes these parameters:
TIP:
For the 1756 digital diagnostic output devices, if the connection is configured for Rack, the diagnostic configuration and I/O data are not supported; if the connection is configured for Data, the diagnostic configuration and I/O data are supported. The supported diagnostics are determined by the catalog number.
Parameter | Description |
|---|---|
Output State During Program Mode | Specifies the behavior of each output when the controller transitions to Program mode.
|
Output State During Fault Mode | Specifies the behavior of the output of each point after a communication fault occurs and the device enters Communications Fault mode.
|
Enable Diagnostics for Field Power Loss | Enables the detection of the loss of field power to the digital output device. This diagnostic is available only for 1756 Digital AC diagnostic output devices. |
Enable Diagnostics Latching | Configures each point on the device to latch diagnostic members so that they remain set after they are triggered. |
When Communication Fails in Program Mode | Specifies the behavior of the outputs if communications fail in Program mode:
|
Provide Feedback