Sensor
Information - Active Type
(class 0x311, instance 1-4, attribute 2)
Configured sensor type.
Value | Sensor Type |
|---|---|
0 | --- |
1 | Oxygen (amp.) |
2 | Oxygen (opt.) |
3 | pH Glass |
4 | E_SensorKSG2_deprecated |
5 | pH ISFET |
6 | Cond c |
7 | Cond i |
8 | ORP |
9 | TU/TS |
10 | Nitrate |
11 | ISE (CAS40D) |
12 | SAC |
13 | Ultrasonic interface (CUS71D) |
14 | Chlorine (CCS142D) |
15 | E_SensorFSPH1 |
16 | E_SensorFSLC1 |
17 | E_SensorFSLI1 |
18 | pH/ORP |
19 | Cond c 4-pol |
20 | Oxygen (opt.) |
21 | TU |
22 | Inline photometer |
23 | TU/AU |
24 | Disinfection |
25 | Spectrometer |
26 | Oxygen (amp.) |
27 | E_SensorKSR2_deprecated |
28 | Fluorescence |
29 | ISE (CAS41E) |
30 | Ultrasonic interface |
31 | DPD Analyzer module |
Information - Serial Number
(class 0x311, instance 1-4, attribute 5)
The serial number of the sensor.
Information - Connected Type
(class 0x311, instance 1-4, attribute 3)
Connected sensor type. The connected sensor type shall match the configured sensor type.
Value | Connected Sensor Type |
|---|---|
0 | --- |
1 | Oxygen (amp.) |
2 | Oxygen (opt.) |
3 | pH Glass |
4 | E_SensorKSG2_deprecated |
5 | pH ISFET |
6 | Cond c |
7 | Cond i |
8 | ORP |
9 | TU/TS |
10 | Nitrate |
11 | ISE (CAS40D) |
12 | SAC |
13 | Ultrasonic interface (CUS71D) |
14 | Chlorine (CCS142D) |
15 | E_SensorFSPH1 |
16 | E_SensorFSLC1 |
17 | E_SensorFSLI1 |
18 | pH/ORP |
19 | Cond c 4-pol |
20 | Oxygen (opt.) |
21 | TU |
22 | Inline photometer |
23 | TU/AU |
24 | Disinfection |
25 | Spectrometer |
26 | Oxygen (amp.) |
27 | E_SensorKSR2_deprecated |
28 | Fluorescence |
29 | ISE (CAS41E) |
30 | Ultrasonic interface |
31 | DPD Analyzer module |
Information - HW version
(class 0x311, instance 1-4, attribute 6)
Hardware version of the device.
Information - SW version
(class 0x311, instance 1-4, attribute 7)
Software version of the device.
Information - Enabled
(class 0x311, instance 1-4, attribute 1)
On: The channel display is switched on in the measuring mode
Off: The channel is not displayed in the measuring mode, regardless of whether a sensor is
connected or not.
Value | Channel Enable |
|---|---|
0 | On |
1 | Off |
Information - Tag
(class 0x311, instance 1-4, attribute 4)
"Tag" stands for the name of a measuring point, and is used in many areas of
process measuring technology. If the TAG control function is activated, the controller
checks every sensor to be connected as to whether this sensor belongs to the measuring
point, and only accepts the sensors that have the same tag.
Operating Time - Total
(class 0x311, instance 1-4, attribute 31)
Operation time of the sensor in seconds.
Operating Time - Initial operation date
(class 0x311, instance 1-4, attribute 11)
Initial operation date of the sensor.
Operating Time - Above spec. temp.e
(class 0x311, instance 1-4, attribute 32)
Total time the sensor is operated above its maximum operation temperature.
Operating Time - Below spec. temp.
(class 0x311, instance 1-4, attribute 33)
Total time the sensor is operated below its minimum operation temperature.
Data Set Switch - SAC
(class 0x311, instance 1-4, attribute 41)
Calibration data records are saved under an individual name in the sensor. A new sensor is
calibrated at the factory and thus already has appropriate data records. You can add your
own data records during each calibration. These are then available for selection under
"Application".
Value | Data Set |
|---|---|
0 | E_DSID_Factory |
1 | E_DSID_NICustomer1 |
2 | E_DSID_NICustomer2 |
3 | E_DSID_NICustomer3 |
4 | E_DSID_NICustomer4 |
5 | E_DSID_NICustomer5 |
6 | E_DSID_NICustomer6 |
7 | E_DSID_NIUndefined |
Data Set Switch - Nitrate
(class 0x311, instance 1-4, attribute 42)
Calibration data records are saved under an individual name in the sensor. A new sensor is
calibrated at the factory and thus already has appropriate data records. You can add your
own data records during each calibration. These are then available for selection under
"Application".
Value | Data Set |
|---|---|
0 | E_DSID_Factory |
1 | E_DSID_NICustomer1 |
2 | E_DSID_NICustomer2 |
3 | E_DSID_NICustomer3 |
4 | E_DSID_NICustomer4 |
5 | E_DSID_NICustomer5 |
6 | E_DSID_NICustomer6 |
7 | E_DSID_NIUndefined |
Data Set Switch - Turbidity
(class 0x311, instance 1-4, attribute 43)
Calibration data records are saved under an individual name in the sensor. A new sensor is
calibrated at the factory and thus already has appropriate data records. You can add your
own data records during each calibration. These are then available for selection under
"Application".
Value | Data Set |
|---|---|
0 | E_DSID_FactoryFNU |
1 | E_DSID_FactoryKaolin |
2 | E_DSID_FactorySIO2 |
3 | E_DSID_FactoryTIO2 |
4 | E_DSID_FactARALeakage |
5 | E_DSID_FactARASludge |
6 | E_DSID_FactARASludgeActiv |
7 | E_DSID_TUCustomer1 |
8 | E_DSID_TUCustomer2 |
9 | E_DSID_TUCustomer3 |
10 | E_DSID_TUCustomer4 |
11 | E_DSID_TUCustomer5 |
12 | E_DSID_TUUndefined |
13 | E_DSID_FactoryLDSludgeActive |
14 | E_DSID_FactoryPSL |
15 | E_DSID_FactoryKieselguhr |
16 | E_DSID_TUCustomer6 |
17 | E_DSID_FactoryAU |
18 | E_DSID_DoNotUseThisSludge |
19 | E_DSID_EBC |
20 | E_DSID_Milk |
21 | E_DSID_Apha |
22 | E_DSID_EBCColor |
23 | E_DSID_OEM1 |
24 | E_DSID_OEM2 |
25 | E_DSID_OEM3 |
26 | E_DSID_OEM4 |
27 | E_DSID_OEM5 |
28 | E_DSID_OEM6 |
29 | E_DSID_Productloss |
30 | E_DSID_Sludge |
31 | E_DSID_AutoSludge |
32 | E_DSID_TUCustomer7 |
33 | E_DSID_TUCustomer8 |
34 | E_DSID_Thickener |
Provide Feedback