Loading
CASE STUDY | LIFE SCIENCES
Recent ActivityRecent Activity

Probiotical S.p.A. Creates Solid Foundation for Expansion-Driven Digital Transformation

Leading Italian probiotics company maintains and improves manufacturing metrics, while scaling its operations, thanks to FactoryTalk InnovationSuite solutions and Rockwell Automation domain experience

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
production machine
probiotical logo

Probiotical is an Italian family-owned company specialized since 1985 in probiotics manufacture, from the raw material to the finished products, with very high quality, guaranteed stability and scientifically backed strains. It drives innovation in a variety of functionalities and technologies, offering customers wide opportunities of customization and range extensions for probiotic blends and finished products ready-to-market, either under Probiotical's brand or in private label.

Challenge

Rapidly rising demand for its products is driving Probiotical to expand its manufacturing and packaging capabilities. But it needs to keep a very close eye on operational data to ensure this expansion is as effectively deployed and managed as possible.

Solution

A Rockwell Automation solution was installed, which included:

  • ThingWorx IIoT solution, part of the FactoryTalk® InnovationSuite
Result
  • Initially considered for a new plant, Probiotical is also collecting and leveraging data from its existing operations
  • Machine availability increased by 15-20%
  • Operational equipment effectiveness OEE near optimum value
  • Reduced energy consumption
  • Reduced packaging waste

Probiotical S.p.A., a leading Italian probiotic and postbiotic research and manufacturing company, was enjoying a huge rise in demand for its products and knew that it had to ramp up production significantly.

With ambitious foresight, it realized that it needed to accelerate its digital transformation across its entire production facilities. This would allow it to more effectively scale its operations and then run them as efficiently as possible, extracting the highest possible yield from its fermenters and packaging lines,

Rockwell Automation specialists were asked to identify and propose the best solution for Probiotical’s shopfloor data management for daily operations, and for integrating IT and OT landscapes. As a result, ThingWorx IIoT solution, part of the FactoryTalk® InnovationSuite, powered by PTC, has been identified and selected as the ideal solution to build  the foundation for its ongoing digital transformation.

Challenge

Probiotical was experiencing exponential growth in demand for its diverse selection of probiotic and postbiotic strains and blends, with supplement-stick volumes rising from 1.5 million per annum up to 10 million.

With this level of growth, the company knew that it needed to establish incredibly tight operational data accuracy and actionable insights, to help ensure that any hard-fought economies of scale were not lost through inefficiency and waste. It also had to integrate new packaging lines with its existing assets and tie these into the optimized manufacturing flows.

“Initially we had very little joined-up visibility into our operations from a holistic perspective,” explains Gianmaria Camanna, COO at Probiotical. “But we knew that if we could get access to pertinent real-time and historic operational data, we would gain a far deeper understanding and, as a result, could undertake work to enhance our operations. Visibility is the key.”

Solution

“Probiotical needed to move quickly,” said Antoine Pris, Director of Enterprise Software Sales at Rockwell Automation. “As demand for its products accelerated, the company recognized that digital transformation would create a robust foundation to support its rapid expansion. This transformation would not only scale its operations but also ensure that time to market, efficiency, quality, and throughput were optimized.”

“We needed the right solution with the right level of support, and we needed a knowledgeable company to help us,” Camanna elaborates. “We quickly recognized the capabilities and value of the FactoryTalk InnovationSuite software. Rockwell Automation was selected to support us due to its industry expertise in food supplements, medical devices and drugs, as well as its software solutions and local system integrator support.”

The ThingWorx IIoT solution can connect a diverse array of disparate devices, applications and data sources, and then bring the resulting data to a single source so it can be aggregated and contextualized based on transactional information from ERP systems. This single source of truth allows users to manage, monitor and control a broad array of automation devices and software applications through one intuitive user interface.

Originally considered as a software cornerstone for a new highly digitalized plant to be commissioned in the summer of 2025, the deployment of the ThingWorx IIoT solution was expanded to include data capture from assets at an existing plant.

“As the project evolved, we realized that we could leverage data from our existing plant,” Camanna explains. “Not only does this give us some significant early wins, but it also gives us the chance to understand the platform in a real-world scenario before we roll it out to our new plant. As a result, we will be able to get to value far quicker at the new plant.”

Result

Initial results highlight that machine availability and operational equipment effectiveness (OEE) are now highly optimized, being within a few percentage points of maximum, with availability seeing a 15-20% increase overall. Further fine tuning is ongoing to ensure these figures can be maintained and even improved.

In addition to these impressive performance metrics, Probiotical is also addressing its sustainability challenges through closer monitoring, which has seen energy consumption and packaging waste cut due to proactive intervention.

With sustainability being a key pillar to the company’s overall strategy, this link between MES information and ESG goals is not only driving its sustainability program forward, but is also giving the company the insights it needs to improve it even further.

Probiotical has a very people-centric approach, so it was essential that its operators and supervisors – and their interactions – were factored into the design and operation of the system, so they could embrace it as a tool that would empower their day-to-day roles. This was achieved in the solution deployed, as its operators now have much better insights into the production process, including the critical fermenters, which define the production volumes and yield. Armed with these insights, the operators and supervisors can make better-informed real-time decisions that can have an immediate positive impact on production.

Published June 27, 2025

Topics: Life Sciences
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies
  5. Chevron LeftChevron Left Solid Foundation for Expansion-Driven Digital Transformation
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose