Loading
Blog
Recent ActivityRecent Activity

Transforming Data for Operational Excellence through Machine Learning and Predictive Analytics

Improve production, quality and maintenance using data you may already have

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Factory workers in PPE looking at paperwork

When an emergency chiller was being incorrectly triggered by changes in the primary chiller’s coefficient of performance (COP), a pharmaceutical company approached Transition Technologies PSC to find a solution. As a trusted Rockwell Automation system integrator, TT PSC worked with three years of historical chiller and environmental condition data available via FactoryTalk® Historian software.

The goal: Predict future COP for the main chiller to alert operators when start of the emergency chiller was required. The team worked to develop a time-series machine learning (ML) model that very precisely predicts COP value within six hours based on the previous 48 hours; integrated the model with real time data in the IoT platform; and deployed continuous calculations to trigger alerts and notify the operations manager when the forecasted COP value exceeds the set threshold.

The result: Model accuracy better than 98% and prediction errors (RMSE) less than 5%. Prediction of COP value six hours in advance.

What can AI/ML do for you?

Using artificial intelligence (AI) or the ability of a computer or computer-controlled robot to perform tasks commonly associated with people, ML or the capability of a machine to imitate intelligent human behavior, manufacturers can boost performance with:

Up to 10% Reduced Downtime – Anticipate equipment faults using predictive rather than reactive maintenance and receive warnings when equipment is operating out of normal ranges.

Up to 12% Better Quality – Earlier detection of process or material faults

Up to 30% More Productivity – Reduced rework and scrap, efficient maintenance planning and greater awareness of process issues

According to Randy Thompson, Senior Business and Solution Architect for TT PSC, ML algorithms build a mathematical model based on available data to make predictions or decisions without being explicitly programmed to do so. During the model building process, historical data is used as an input to train the model – typically 70% for training and 30% held back for evaluation and confirmation of the model.

What makes a good ML use case?

A good ML use case consists of a measurable prediction goal, many variables and available historical data. Companies usually have a lot of data, but often not the data they need to predict the goal they’d like to achieve. This may require additional sensor inputs or modifying the prediction goals. This is an area where having an experienced partner can help.

A good ML use case example is a wood drying process with the goal of getting the wood to a certain moisture content. With ML you can input all the measurable variables from the process to predict what speed to operate the dryer to achieve the correct drying level. What’s great about machine learning, says Thompson, is that after you add the needed data, the model will do the work for you. Other questions to determine include:

  • Is this a problem worth addressing? What’s the expected business benefit?
  • How often does the issue occur? Best case scenario is that it occurs regularly enough to give you sufficient data to create a model and see results.
  • What is the cost in downtime?
  • What will you do differently if you have this prediction?

Finally, do you have the data needed to build the model? It begins with a hypothesis. Choose what you think is important rather than feeding in all the data. Next, ask what data is available and is there enough data to make an accurate prediction.

Using the Analytics Accelerator for FactoryTalk Historian

Analytics Accelerator for FactoryTalk Historian is a combination of tools that Rockwell Automation has developed to assist manufacturers in doing their own modeling.

It’s an Integrated Portfolio Solution built using ThingWorx® to make it easier to apply ML to data stored in FactoryTalk Historian data archives. The solution consists of several services and ThingWorx mashups which make up the user interface.

Analytics Accelerator for FactoryTalk Historian graphic

The solution is built following the building block model, with the intention of making it easier to develop additional functionality on top of the existing features. The following features are supported:

  • Easily apply analytics and machine learning to data stored in the archive
  • Analyze historical and live data from your FactoryTalk Historian
  • Harness the power of an IIoT platform with built in analytics and machine learning capabilities
  • Intuitive analytical tools accessible to operational experts
  • Step-by-step guidance for common manufacturing and device-specific use cases
  • Out-of-the-box functionality informed by decades of industrial experience

The extension requires simple installation and configuration steps in ThingWorx to connect existing FactoryTalk Historian data and configure ThingWorx Analytics (a product add-on to ThignWorx) capabilities. The provided user interface via ThingWorx allows users to easily define and analyze data models.

“This is a technology stack that you put together and then get started adding data into the models. One of the great features is that you can do this without a data scientist. You’ll learn about the process and find many uses for it,” Thompson said.

Start building your own ML models

Improve production, quality and maintenance using data you may already have with FactoryTalk Historian, Analytics Accelerator for FactoryTalk Historian and the Rockwell Automation team. Contact Transition Technologies PSC at ttpsc.com.

Published July 17, 2024

Topics: Accelerate Digital Transformation Optimize Production Data Science & Industrial Analytics Digital Transformation Smart Manufacturing Artificial intelligence FactoryTalk Historian Thingworx IIoT

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Transform Data Using AI for Operational Excellence