Save System History

When you save system history, the RMCT saves all event log entries to a ZIP file with two CSV files: one for the connected redundancy module and one for the partner redundancy module.
To save system history, follow these steps.
  1. On the Event Log tab, select Save System History.
    Save System History button on Event Log tab of RMCT
  2. Browse to the location where you want to save the ZIP file and select Export.
    Export Event Log dialog box
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal