Edit SFC routine properties

Use the
Routine Properties
dialog box to edit the properties of a sequential function chart routine.
To edit SFC routine properties
  1. In the
    Controller Organizer
    , right-click the routine and select
    Properties
    to open the
    Routine Properties
    dialog box.
  2. In the
    Name
    box, type a name for the sequential function chart routine.
  3. In the
    Description
    box, enter a description of the routine.
  4. Select the
    Auto-Naming
    tab to configure auto-naming settings. Auto-naming generates names for language elements in the routine.
  5. Select the
    Sheet Layout
    tab to configure the sheet size and orientation for the routine.
  6. To apply a set of permissions to the routine, select a
    Permission Set
    . The permission set controls access to the routine based on the permissions configured in FactoryTalk Administration Console. The default setting,
    <Controller Inherited>
    , applies the same security settings that have been applied to the controller or project.
  7. Select
    OK
    .
    TIP:
    The
    Auto-Naming
    and
    Sheet Layout
    tabs only display on the
    Routine Properties
    dialog box for unprotected sequence routines.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal