Error creating <directory name>

Error creating the directory. This could be because:
  • The drive does not exist.
  • The user does not have creation privileges on the specified drive.
  • There is not enough hard disk space.
Enter a valid drive, check administrative privileges, and clear space on the hard drive, as necessary.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal