Coordinate System Properties - Motion Planner

Use the settings on the
Motion Planner
tab in the
Coordinate System Properties
dialog box to:
  • Enable or disable Master Delay Compensation.
  • Enable or disable Master Position Filter.
  • Enter the bandwidth for the Master Position Filter.
The
Motion Planner
tab is available only when configuring a Cartesian coordinate system.
TIP: To open the Motion Planner tab:
  1. In the
    Controller Organizer
    , expand the
    Motion Group
    folder, and double-click the coordinate system.
  2. On the
    Coordinate System Properties
    dialog box, click the
    Motion Planner
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal