Acceleration Loop page
Use the settings on the
Acceleration Loop
page to configure the acceleration loop of the axis. The axis configuration and information from the drive's profile determine the options that appear on the page.
TIP:
To open the Acceleration Loop page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickAcceleration Loop.
Parameter | Description |
|---|---|
Acceleration Loop Enabled | Enables and disables the acceleration loop. Select the check box to enable the acceleration loop. |
Bandwidth | Specifies a value for the bandwidth in Hertz. |
Integrator Bandwidth | Specifies a value for the integrator bandwidth in Hertz. |
Feedback Gain | Specifies a value for the feedback gain. |
Acceleration Limit | Specifies a value for the acceleration time in Position Units / Sec 2 . |
Deceleration Limit | Specifies a value for the deceleration time in Position Units / Sec 2 . |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.
TIP:
The
Parameter List page may contain
more attributes than the associated page. In some cases, attributes that display
on the Parameter List page do not display on the associated page. |
Provide Feedback