A fault exists in <standard control or safety task>
Click Yes to confirm that you want to clear faults for these scenarios.
A fault exists in standard control.
The controller keyswitch is in RUN, so clearing faults will restart Safety task and standard control execution.
A fault exists in safety task and in standard control.
The controller keyswitch is in RUN, so clearing faults will restart Safety task and standard control execution.
A fault exists in safety task .
Standard control is running, so clearing faults will restart Safety task execution.
A fault exists in safety task and in standard control.
A download is required to clear the Safety fault.
Provide Feedback