Open/Import Project Dialog Box - Source Control View
Use this dialog box to open a project file or to perform a full import of a project file from Source control view.
Parameters
Parameter | Description |
|---|---|
Look in: | Select the directory in the AssetCentre archive where the project to open or import resides. (The last open location is remembered upon subsequent returns.) |
Up One Level - ![]() | Move up one level in the directory tree. Active when logged in to a server or database and if not already at the top level of the tree. |
View Menu - ![]() | Select the view type (view list of file names or list of file names with username). Active when logged in to a server or database. |
Login - ![]() | Log in to a specific server and attach to a specific database. |
Manage Server Registrations - ![]() | Open a dialog box to manage one or more server or database combinations. |
Select Version or Label for the Operation - ![]() | Select an archived element based on either version or a label. Active when file selected. |
Search for Files or Folder - ![]() | Select to search for either files or folders within the current archive database. Active when logged in to a server or database. |
Help - ![]() | View source control help. |
Directory/File | Displays directories and files contained within a specific server or database. The View Menu determines the view type (either list or details). |
Check Out | If unselected, retrieves a copy of the selected file when selecting Get. If selected, the file to retrieve is checked out. Not selected and not active if selected file is already checked out. |
File Name | Displays the currently selected file (read-only). |
Files of type: | Choose the type of file to open or import (ACD file is the only option). |
Get | Retrieve (get) the file or check out the file (if Check Out box is selected). Active if logged in to a server or database and if a file is selected to retrieve. |
Cancel | Cancel the open or import and close the Open/Import Project dialog box. |
Help | View help about Open/Import Project dialog box. |
Provide Feedback