Error - File with same name exists
A writable instance of the file is open in another instance of the
Logix Designer
application. The file was not checked out.Option | Description |
|---|---|
OK | Return to the Open/Import Project dialog box |
Help | Help about this error |
Provide Feedback