Discover Module command

Add a module from a list of modules attached to a given backplane or network. When selected, the
Module Discovery
tab in the
Select Module
dialog box appears.
TIP: The
Discover Module
command is available only when the
Logix Designer
application is online and the network path is valid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal