Search in routines
To search in routines, choose one of the following options:
- Current Routine
- All Routines in Current Instruction (Controller Organizer only)
- All Routines in Current Program / Equipment Phase
- All Routines in Current Task (Controller Organizer only)
- All Routines (note that theAll Routines in Current ProgramorAll Routines in Current Taskoptions do not search Add-On Instruction logic from where it is invoked in routines. Also note that theAll Routines in Current Programoption does not search routines within program hierarchies.)
Provide Feedback