Configure PPTC instructions
Use the
Advanced
tab of the PPTC Properties
dialog box to configure the Pressure/Temperature Compensated Flow (PPTC) instruction. To configure PPTC instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Open theAdvancedtab.
- Set the parameters:
- Flow below which to report zero flow. If Out_Flow is less than this cutoff value, 0.0 appears.
- Reference (full-scale) differential pressure. Reference (full-scale) differential pressure (for example, WC).
- Reference flow in volumetric units at reference DP. Reference flow in volumetric units (for example, CFM) at reference differential pressure (DP).
- Zero input-unit pressure in absolute unit. Zero input-units pressure in absolute units (for example, PSIA).
- Zero input-unit temperature in absolute unit. Zero input-units temperature in absolute units (for example, R or K).
- Standard pressure. Standard pressure in Inp_PAct units (for example, PSIG).
- Standard temperature. Standard temperature in Inp_TAct units (for example, F or C).
- Flow calculation method. 1 = Use Inp_DPAct (square root curve) to calculate flow; 0 = Use Inp_FAct (linear).
- SelectApply.
Provide Feedback