Add Ladder Element dialog box
Use this dialog box to add instructions, rungs, branches, or branch levels to a ladder routine. When entering the instruction mnemonic, the closest match is selected in the list. Place the instruction in a list or a group.
TIP:
To open the open the Add [Language element] dialog:
- Press theAlt + Insertkey.
- ChooseEdit>Add <Language> Element.
TIP:
The appearance of the
Add <Language> Element
dialog varies slightly, depending on the language editor (Ladder, SFC, FBD, structured text) you are using. Refer to the specific language editor dialog boxes for information specific to each language.Add instructions via Quick Keys. Add-On-Instructions cannot be used as a Quick Key.
Parameters | Description |
|---|---|
Ladder Element | Enter the element to add. The ladder element list advances to the closest match. If the project uses a controller that does not have a serial port, the Add Ladder Element dialog box does not show the ASCII Serial Port group, which contains the Serial Port instructions (the ASCII String and ASCII Conversion groups and instructions remain). The user-configured tab order is not affected by the removal of the ASCII Serial Port group. |
Instruction Help | Select to toggle between turning the Instruction Help pane on and off.The Instruction Help pane is operational for built-in instructions and Add-On Instructions. |
Instruction Help Pane | Opens to the right and displays the instruction help. For built-in language elements, a Full Instruction Help for <element> button above the instruction help text navigates to the full instruction help for that instruction.Logix Designer application InstructionOnce the dialog box is expanded to display the help, the Logix Designer application InstructionLadder Element List Available ladder elements include:
If an instruction is not valid for the current context, for example, inside an Add-On Instruction logic routine, the instruction is not in the list. Add-On Instructions that cause recursive calls are in the list, but appear dimmed. |
Show Instructions by Groups | Displays the list in groups to help organize the instructions. Selected by default. When deselected, the instructions appear in alphabetical order. |
New Add-On Instruction | Opens the New Add-on Instruction dialog box. |
Provide Feedback