View the maximum and used Ethernet nodes for a controller
Some controllers have limits on the number of Ethernet nodes they support in the I/O Configuration tree. When a device is added directly to the Ethernet I/O configuration, it is counted toward the node limitation of the controller.
The
Capacity
tab of the Controller Properties
dialog box shows the current number of used Ethernet nodes in the I/O Configuration tree and the maximum number of Ethernet nodes supported by the controller. When the controller is online and the controller enforces the node count, the following occurs when the node count exceeds the limit:
- An error dialog box appears.
- The I/O module cannot be added to the I/O Configuration tree.
When the controller is offline and the controller enforces the node count, the following occurs when the node count exceeds the limit when the project is verified or the controller attempts to go online:
- An error message is generated on theErrortab of theOutput window.
- The project cannot be downloaded to the controller.TIP:The 1756-L85E controllers do not enforce the node count, meaning the system does not prohibit you from connecting additional nodes, and it may be possible to download the project. The system provides a warning when the recommended node limit has been exceeded.
To view the maximum and used Ethernet nodes for a controller:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click theCapacitytab.
- In theEthernet Nodegroup, view the information about the Ethernet nodes.
- Maximum/Recommended Maximum- shows the maximum or recommended maximum number of Ethernet nodes for the controller
- Used- shows the current number of Ethernet nodes in the I/O Configuration tree
If the number of used Ethernet nodes exceeds the maximum number,
appears next to the
Used
parameter when controller is offline. For the 1756-L85E controllers, if the node count exceeds the recommended limit,
appears next to the
appears next to the Used
parameter and the following message appears:The recommended node limit has been exceeded. It may be possible to connect additional nodes depending on the node type and system architecture.
Provide Feedback