Observing a Source Protected Add-On Instruction

Use these steps to verify that source protection is being applied to an Add-On Instruction.
To observe how source protection works:
  1. Rename the sk.dat file to some other name.
  2. Open the project in the
    Logix Designer
    application.
    There is now no valid key file available to this
    Logix Designer
    application project.
    Tip:
    When the Source Key is available, the Add-On Instruction behaves the same as if it were not source protected.
  3. Review how the instruction appears in the Add-On Instructions folder.
    Now the protected Add-On Instruction definition's routines and tag folder are not shown if fully protected, and the definition cannot be edited.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal