Alarm event attributes and values
The attributes and values are not case-sensitive. Use the logic operator
OR
to separate multiple values, for example, Urgent OR High
.The following table shows the available attributes and values that you can use for filtering or sorting.
Attributes | Description | Support filtering? | Support sorting? |
|---|---|---|---|
Priority | The values can be:
| Yes | Yes |
AlarmState | The values can be:
| Yes | Yes |
EventTime | No | Yes | |
AlarmName | Yes | Yes | |
ConditionName | Yes | No | |
Message | Yes | No | |
CurrentValue | No | No | |
LimitValue | No | No |
Provide Feedback