RSTwindowStyle constants
Use the constants with the WindowStyle property.
The following constants are defined:
Constant | Description |
|---|---|
rstWindowStyleDefault | Sets the trend object to a solid background that matches the container’s window color. |
rstWindowStyleOpaque | Sets the trend object to a solid background. |
rstWindowStyleTransparent | Sets the trend object to a transparent background. |
Provide Feedback