The parent of an object
The following table shows the parent for a given object in
FactoryTalk View SE
.Object | Parent |
|---|---|
Application | Application |
Display | Application |
Folder | TagDB or Folders |
Folders | Folder |
Tag 1 | TagGroup |
TagDB | Application |
TagGroup | Application |
1. If the Tag object is returned from the TagDB object, the parent object is Nothing . | |
Provide Feedback