Use rubberband zoom (XY Plot)
Rubberband zooming allows you to zoom in on a time period. For stacked tags, only the tag with focus will zoom while all tags will zoom for overlaid tags.
To use rubberband zoom
- On the toolbar, clickRubberband Zoom
. - Use the cursor to create a rectangular shape on the plot surface in the location you want to zoom in on. The trend updates to fill the plot surface with the area you selected.You can click the plot surface to further zoom into the area.
- When finished zooming in, clickReset View
at the bottom right of the plot surface to reset the plot surface to the original view, while remaining in rubberband zoom mode.
Provide Feedback