Use x-axis cursors (XY Plot)
When the x cursor is enabled, two vertical cursors that slide along the x-axis display. Each cursor can be operated individually. You can also use the x-axis cursor with the y-axis cursor. This feature is useful when you stack the y-axis so you can quickly see the values for a point in time for all traces at once and compare those values.
Cursors:
- Can be used while zooming in on data.
- Allow panning of data.
- Display values of data points that touch the cursor.
To use x-axis cursors
- On the XY Plot toolbar, clickX-axis Cursors
. Two vertical cursors display on the XY Plot. - Drag each cursor left or right on the plot surface. The following information displays:
- Data point values for each trace at the cursor location.
- X tag value difference between two cursors.
Provide Feedback