Transpose axes
Transposing axes switches the x-axis with the y-axis.
To transpose axes
- Do one of the following:
- On the XY Plot toolbar, clickTranspose Axes
. - Right-click the plot surface and clickTag Axes > Transpose.
Provide Feedback