Stack axes (XY Plot)
Stacking axes displays all traces on the plot surface in their own grid, or zone. Each trace will have its own y-axis and x-axis visible. All of the axes can still be moved.
To stack the axes
- Right-click the plot surface, selectTag Axes > Stack, and select one of the following:
- Y-Axes.If more than one trace exists, displays each trace with separate y-axis.TIP:Alternate method for stacking the y-axes:On the XY Plot toolbar, clickStack Tag Y-Axes
. - X-Axes.If more than one trace exists, displays each trace with separate x-axis.
- Both.If more than one trace exists, displays each trace separately in its own grid.
Provide Feedback