Y-Axis page (XY Plot)
How do I open the Y-Axis page (Properties dialog box)?
- On thePropertiesdialog box, click theTracestab.
- Click the tag name in the left pane.
- Click theY-Axisoption.
Y-axis properties allow you to define how the y-axis displays information for the current XY Plot. The properties are applied immediately to the current XY Plot.
TIP:
You can add a new trace or a parameter to the XY Plot by clicking
. Parameters accept a format of #
. Parameters accept a format of #number
, such as #1.The following options are available:
Property | Description | ||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Label | The options to include in the axis label. The following options are available:
| ||||||||||||||||||||||||||||||
Axis | The display options for the axis. Select from the following options:
| ||||||||||||||||||||||||||||||
Scale | The scale used to determine the best display of data. Select one of the following options:
You can quickly switch between the automatic and min/max settings by toggling Automatic Scales in the toolbar. | ||||||||||||||||||||||||||||||
Mode | The scale to use for numeric types. Select from the following options:
| ||||||||||||||||||||||||||||||
Tick marks | The short lines along the axis line that specify value divisions. Select one of the following options:
|
Provide Feedback