Shape page (XY Plot)
How do I open the Shape
page (Properties dialog box)?
- In thePropertiesdialog box, click theGeneraltab.
- ClickShapein the left pane.
Shape properties allow you to set the background, outline, and marker color that displays in the current
XY Plot. This tab only displays if a shape has been added to the plot surface.
The following properties are applied immediately to the current XY Plot.The following options are available:
Property | Description |
|---|---|
Background | The fill color for the shape. Select from the following options:
|
Outline | The color, style, and width of the shape's outline. Select from the following options:
|
Marker | The color of new points when in Edit mode, while editing a shape. Press the CTRL key while clicking a point to change to the new marker color. |
Points | The data points that fall outside of the shape. |
Provide Feedback