Automatically scale XY Plot traces
When creating XY Plot traces, automatic scaling determines a scale for the x-axis and y-axis that will best display the available data. XY Plot evaluates the trace data values and sets the x-axis and y-axis values based on the minimum and maximum data values to display.
To automatically scale an XY Plot
- On the XY Plot toolbar, clickAutomatic Scales
.TIP:If you have manually defined Min/Max values for any tags on the XY Plot, enabling automatic scaling will remove those values.
Provide Feedback