Add traces at runtime (XY Plot)
At runtime, you can add a trace with a pair of tags
to the XY Plot. Traces added at runtime are not saved.
For each trace on an XY Plot object, samples are plotted using horizontal x-axis representing one tag value and a vertical y-axis representing another tag value.
TIP:
To show data from FactoryTalk View SE data logs, make sure the data log models are started. Otherwise, the trend will not show any value of your selected tags.
To trend historical data in
a FactoryTalk Historian
SE server, Asset Framework server, FactoryTalk Historian ME module, or PI Server
, you
need to install FactoryTalk Historian Connectivity
from the FactoryTalk View
installation package on the FactoryTalk View Studio or SE Client computer.All clients must use either the same computer name or the same IP address. If you add or delete a PI server, restart your FactoryTalk View Studio or FactoryTalk View SE Client to take effect.
To add traces to an XY Plot at runtime from the chart
- On theTag Explorerpane of the chart, expand the tree and navigate to the folder for the data source.
- On theItemspane, drag one tag as the x tag and another as the y tag to the chart.
To add traces to an XY Plot at runtime from the context menu
- On the chart, right-click and selectProperties.
- On theTracestab, click
. - In theAdd Tracedialog box, click theX Tagbrowse button.
- On theTag explorer, expand the tree and navigate to the folder for the data source.
- On theItemspane, select one tag.
- ClickOK.
- In theAdd Tracedialog box, click theY Tagbrowse button and repeat the steps in Step 3.
- ClickOK.
Provide Feedback