Commands used with input objects
You can use the following commands with input objects at runtime.
Commands | Description |
|---|---|
DownLoad | Downloads the contents of the selected input object to a tag in a database or external device. |
DownLoadAll | Downloads the contents of all input objects in the current graphic display to tags in a database or external device. |
UpLoad | Reads a value from a tag in a database or external device and displays it in the selected input object. |
UpLoadAll | Reads values from tags in a database or external device and displays them in the input objects in the current graphic display. |
Provide Feedback