Options on the Template tab
The following table shows the options on the
Template
tab.Options | Descriptions |
|---|---|
Select template options | Designates which options from each Trend property tab to save with the selected template and apply when the template is loaded. Click a tab name in the left panel to see a list of associated options in the right panel. To save an option with the template, select its check box in the right panel. |
Check All | Click Check All to select all options for the selected tab. |
Uncheck All | Click Uncheck All to clear all options for the selected tab. |
Default | Click Default to return to the system-set default settings for the selected tab. |
All options | Select All Options and then select Check All , Uncheck All , or Default to change all of the tabs at once. |
Provide Feedback