Options on the Runtime tab
The following table shows the options on the Runtime tab.
Options | Descriptions |
|---|---|
Display property tabs | Allows you to specify which trend property tabs are available to operators at runtime. Runtime property tabs include the General, Display, Pens, X-Axis, Y-Axis, Overlays, and Template tabs. The Runtime tab is not available at runtime. |
Chart behavior | These options determine what happens when an operator clicks, or double-clicks the trend at runtime. |
Allow editing legend properties | Select this check box to allow operators to change trend legend options at runtime. The operator can double-click the trend chart legends at runtime to open the corresponding trend properties tab. At least one of the following tabs must be selected in the Display property tabs option to allow editing legend properties: Pens tab, X-Axis tab, or Y-Axis tab. If the tab is not selected, the operator cannot open that tab at runtime by clicking the trend legend. |
Allow Pan/Zoom | When selected, allows operators to zoom, and pan on the runtime chart. To disable zooming and panning, clear the check box. |
Context menu options | Determines which options are available on the context menu when operators right-click the trend at runtime. |
Allow Pause/Resume scrolling | When selected, allows operators to pause and resume automatic scrolling from the context menu. |
Allow Show/Hide value bar | When selected, allows operators to show and hide a value bar from the context menu. |
Allow snapshot creation | When selected, allows operators to create and name a snapshot, for use as an overlay. |
Allow overlay options | When selected, allows operators to select snapshots, and add them to the trend as overlays, and to show and hide selected overlays. |
Allow print | When selected, allows operators to print the trend chart. |
Allow Delta value bar | When selected, allows operators to use a second value bar to calculate the difference between two x-axis points on a trend chart. |
Allow Export trend data | When selected, allows operators to export the trend data into a CSV file. Note: Historical data is retrieved for the time span of the trend and the data may be condensed to show properly on the trend. Exporting the trend data will reflect actual data, but in the condensed format. |
Allow Export Datalog Model data | When selected, allows operators to export the data log model data into a CSV file, for example, 20160127_1200_50_363_hs_dlm.csv where hs is the name of the HMI server and dlm is the name of the data log model.If you have multiple data log models in the trend, each data log model is saved into one CSV file. |
Provide Feedback